Issues in SPI Boot on custom T2081

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issues in SPI Boot on custom T2081

1,262 Views
Irfan3
Contributor III

Hi Team,

We are working on SPI NOR boot in T2081 custom board.
 
We were able to load the U-boot into the SPI NOR device and it was running till DDR Initialization failed.
 
While DDR debug due to DDR init fail, with some changes in hardware, now we are not able to boot-up at all.
 
We have cross checked the dump of the flashed file with the input file and it's same. Also, we have checked the loaded file and configuration of PBL from software side, it's not changed at all.
 
Could you please suggest us how to debug this issue.
 
Thanks and Regards,
Irfan
0 Kudos
Reply
1 Reply

1,252 Views
ufedor
NXP Employee
NXP Employee

> While DDR debug due to DDR init fail, with some changes in hardware

Which exactly hardware changes?

0 Kudos
Reply