Hello,
We are having problems with a MPC8306 input pins configuration while PORESETsignal is active. The issue is that pins configured as inputs are not acting as input as expected and they have a logic 1 value instead.
¿Any idea about what's happening?
Thanks in advance.:smileyblush:
Any other sugestion?
 
					
				
		
 LPP
		
			LPP
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		There might be due to improper functioning of JTAG/COP port. Please, check if the port connections comply Freescale recommendations in AN4231 Design Checklist for MPC8306 Processor.
Critical things:
- PORESET should cause TRST
- pull-ups on TCK. It does not have an internal pull-up, and requires an external one if not used. There is a pullup on TMS but it is always safer to put a pullup on TCK however, because then we will not have a floating input.
.
 
					
				
		
 LPP
		
			LPP
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Please, refer to section 2.2 "Power Sequencing" of MPC8306EC:
"if the I/O voltages are supplied before the core voltage, there might be a period of time that all input and output pins are actively driven and cause contention and excessive current. In order to avoid actively driving the I/O pins and to eliminate excessive current draw, apply the core voltage (VDD) before the I/O voltage (GVDD and OVDD) and assert PORESET before the power supplies fully ramp up".
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Just to clarify the situation:
PORESET is not a Power up reset but a warm reset initiated by user after system is steady.