I2C Problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C Problem

1,873件の閲覧回数
mohsenhaghighat
Contributor III

Hello,

We design a Backplane system with PCA9548A I2C switch,  In this design, the I2C switch multiplex I2C between cards. when write 0x00 in register 0 of PCA9548A, and output I2C ports are disable, the I2C signal is OK!

But when wite 0xff in resister 0 of PCA9548A, and output I2C ports are enable, the I2C signal is not OK because the low level of the signal come to 0.7 volt. What can I do to overcome this problem?

I attach I2C signal Image, whan all ports are enable and all ports are disable.

thanks

タグ(1)
0 件の賞賛
返信
1 返信

1,732件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please explain how the issue is related with a PowerQUICC processor.

0 件の賞賛
返信