I2C Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I2C Problem

1,207 Views
mohsenhaghighat
Contributor III

Hello,

We design a Backplane system with PCA9548A I2C switch,  In this design, the I2C switch multiplex I2C between cards. when write 0x00 in register 0 of PCA9548A, and output I2C ports are disable, the I2C signal is OK!

But when wite 0xff in resister 0 of PCA9548A, and output I2C ports are enable, the I2C signal is not OK because the low level of the signal come to 0.7 volt. What can I do to overcome this problem?

I attach I2C signal Image, whan all ports are enable and all ports are disable.

thanks

Tags (1)
0 Kudos
Reply
1 Reply

1,066 Views
ufedor
NXP Employee
NXP Employee

Please explain how the issue is related with a PowerQUICC processor.

0 Kudos
Reply