How to enable Second UART in MPC8323E-RDB board.?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to enable Second UART in MPC8323E-RDB board.?

1,319 次查看
narreddisivapra
Contributor II

Hello,

         Can anyone suggest how to enable the Second UART in MPC8323E-RDB board.? Is there any possibility in enabling UART while configuring Kernel using LTIB.?

         Please suggest relevant document available, if any.

         I am using LTIB to build Kernel and rootFs images. Please respond as soon as possible.

Thanks and Regards,

Siva Prakash Reddy N

标记 (2)
0 项奖励
回复
2 回复数

1,184 次查看
Pavel
NXP Employee
NXP Employee

The MPC8323 DUART is enabled in the MPC832x_rdb LTIB Linux BSP. Attached file contains .dts file from this BSP. This file is available using the following path:

ltib-mpc832x_rdb-20081112/rpm/BUILD/linux-2.6.20/arch/powerpc/boot/dts

 

Find definition for serial0 and serial 1 in this file.

This file shows that both UARTs are enabled in this BSP.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,184 次查看
narreddisivapra
Contributor II

Thanks for the response. Can you please explain how can I access the second UART available on the board.?

Thanks and Regards,

Siva Prakash Reddy N

0 项奖励
回复