How to Add RT-Linux Patch

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to Add RT-Linux Patch

跳至解决方案
4,034 次查看
narreddiprakash
Contributor II

Hello,

         I am using LTIB for Kernel image building for the bsp "MPC8360EA-MDS-RDB" and I am using ubuntu 9.04 loaded PC. I built LTIB successfully, but the built kernel not supporting RT-Linux. So, how can I add RT-Linux patch for this BSP using LTIB.?

Please respond as soon as possible.

Thanks

Prakash

标记 (1)
0 项奖励
回复
1 解答
3,820 次查看
Pavel
NXP Employee
NXP Employee

In fact, our Linux kernel is a standard Linux kernel, we just add some driver into it. So default, it's a preemptive kernel. All of Linux kernel supports preemp in kernel control path.See attached file.
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,820 次查看
narreddiprakash
Contributor II

Thanks for suggestion. I already built kernel for MPC8323e-rdb board where it has a "kernel-2.6.20-rt8" option.

but here in this MPC8360EA-MDS-PB kernel building has no such option. What is the main difference between theses two.?

Regards,

Prakash

0 项奖励
回复
3,820 次查看
narreddiprakash
Contributor II

please reply to this query.

0 项奖励
回复
3,821 次查看
Pavel
NXP Employee
NXP Employee

In fact, our Linux kernel is a standard Linux kernel, we just add some driver into it. So default, it's a preemptive kernel. All of Linux kernel supports preemp in kernel control path.See attached file.
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,820 次查看
Pavel
NXP Employee
NXP Employee

In fact, our Linux kernel is a standard Linux kernel, we just add some driver into it. So default, it's a preemptive kernel. All of Linux kernel supports preemp in kernel control path.See attached file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复