How to Add RT-Linux Patch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Add RT-Linux Patch

ソリューションへジャンプ
3,916件の閲覧回数
narreddiprakash
Contributor II

Hello,

         I am using LTIB for Kernel image building for the bsp "MPC8360EA-MDS-RDB" and I am using ubuntu 9.04 loaded PC. I built LTIB successfully, but the built kernel not supporting RT-Linux. So, how can I add RT-Linux patch for this BSP using LTIB.?

Please respond as soon as possible.

Thanks

Prakash

タグ(1)
0 件の賞賛
返信
1 解決策
3,702件の閲覧回数
Pavel
NXP Employee
NXP Employee

In fact, our Linux kernel is a standard Linux kernel, we just add some driver into it. So default, it's a preemptive kernel. All of Linux kernel supports preemp in kernel control path.See attached file.
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,702件の閲覧回数
narreddiprakash
Contributor II

Thanks for suggestion. I already built kernel for MPC8323e-rdb board where it has a "kernel-2.6.20-rt8" option.

but here in this MPC8360EA-MDS-PB kernel building has no such option. What is the main difference between theses two.?

Regards,

Prakash

0 件の賞賛
返信
3,702件の閲覧回数
narreddiprakash
Contributor II

please reply to this query.

0 件の賞賛
返信
3,703件の閲覧回数
Pavel
NXP Employee
NXP Employee

In fact, our Linux kernel is a standard Linux kernel, we just add some driver into it. So default, it's a preemptive kernel. All of Linux kernel supports preemp in kernel control path.See attached file.
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
3,702件の閲覧回数
Pavel
NXP Employee
NXP Employee

In fact, our Linux kernel is a standard Linux kernel, we just add some driver into it. So default, it's a preemptive kernel. All of Linux kernel supports preemp in kernel control path.See attached file.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信