How can I install Codewarrior v8.8 in linux OS(Ubuntu 16.04)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I install Codewarrior v8.8 in linux OS(Ubuntu 16.04)

1,252件の閲覧回数
jinyu_zhang
Contributor II

I'm attemping to install codewarrior IDE in Ubuntu16.04. But I get the installation package from NXP as an exe file. How can I install it into the target OS?

0 件の賞賛
返信
2 返答(返信)

1,157件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use Ubuntu 10 or Ubuntu 12 for installing CodeWarrior 8.8 for Linux.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,157件の閲覧回数
jinyu_zhang
Contributor II

As I can only get the Windows-hosted installation package for version 8.8, which is .exe file.

Is it suitable to install in Ubuntu?

0 件の賞賛
返信