How can I install Codewarrior v8.8 in linux OS(Ubuntu 16.04)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How can I install Codewarrior v8.8 in linux OS(Ubuntu 16.04)

1,242 次查看
jinyu_zhang
Contributor II

I'm attemping to install codewarrior IDE in Ubuntu16.04. But I get the installation package from NXP as an exe file. How can I install it into the target OS?

0 项奖励
回复
2 回复数

1,147 次查看
Pavel
NXP Employee
NXP Employee

Use Ubuntu 10 or Ubuntu 12 for installing CodeWarrior 8.8 for Linux.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,147 次查看
jinyu_zhang
Contributor II

As I can only get the Windows-hosted installation package for version 8.8, which is .exe file.

Is it suitable to install in Ubuntu?

0 项奖励
回复