FS8530 Vpre Not Output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS8530 Vpre Not Output

2,368件の閲覧回数
jhhan
Contributor I

HI~

Now I use FS8530 PMIC
VBOS => VPRE => VBoost => BUCK1/BUCK2/BUCk3/LDO1/LDO2
The power supply operates normally with the WakeUP 1 signal.
I have a problem.
When powered off, change the PMIC to GotoStandby.
However, if the Wakeup1 signal occurs due to quick power application,

the Vpre power is not output. (Most normal working)
Current register settings changes, do not solve the problem.
I would appreciate it if you could let me know if there is a solution.

0 件の賞賛
返信
4 返答(返信)

2,340件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

HI 

Please help and check whether you match below red circled conditions to turn on Vpre:

guoweisun_0-1723016202950.png

 

0 件の賞賛
返信

2,334件の閲覧回数
jhhan
Contributor I

Thank you for your quick response.

1. Wake1 = '1' DBG = '0' , I think go to Next

2. VSUP > VSUP_uvh: OK

  VBOS > VBOS_uvh : OK

I don't know the condition that FS_READY '1'

Psync is '0' when measured with an oscilloscope.

The OTP setting is shown in the attached figure.

 

 

0 件の賞賛
返信

2,298件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

 FS_READY '1' means A synchronization between Main and Fail safe state machines, which is indeed VSUP > VSUP_UVH and WAKE1
or WAKE2 > WAKE12VIH, and LBIST has been executed

0 件の賞賛
返信

2,331件の閲覧回数
jhhan
Contributor I

attached figure

0 件の賞賛
返信