Ethernet not working properly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Ethernet not working properly

3,703件の閲覧回数
jagrati_chaudhary
Contributor II

i upgraded my device kernel 4.1 to 6.1 which use soc LS1020A. after upgrade device id booting properly and Ethernet poet is coming up but when i try to ping Ethernet server using Ethernet  port ping is not going even i am using the same Ethernet port which i use to boot device using tftp boot.

i added my device dts and dtsi file and kernel logs also.  

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,560件の閲覧回数
jagrati_chaudhary
Contributor II

Is there any way that i can upgrade my device Kernel without upgrade uboot? 

0 件の賞賛
返信

3,669件の閲覧回数
Oswalag
NXP TechSupport
NXP TechSupport

Hello.

You upgraded to 6.1 but in your log file I see the U-boot version as 

U-Boot 2016.09

Please as a first step, upgrade your u-boot  version according to the LLDP version.