Drivers for the MPC860

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Drivers for the MPC860

1,468 Views
maheshwarreddy
Contributor I

Hai,

We are using the MPC860 processor. we need the drivers for the processor. we need drivers for the SPI,UART and parellel interface can you please provide the drivers.(IDE code warrior 8.0  )

Thank you 

Best regards

Maheshwar.

0 Kudos
Reply
1 Reply

1,341 Views
Pavel
NXP Employee
NXP Employee

See simple program examples in the attached file.

If there is a problem for .zip or 7z file loading, create please technical case:

https://community.nxp.com/thread/381898


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply