Drivers for the MPC860

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Drivers for the MPC860

1,493 Views
maheshwarreddy
Fresh Out Contributor

Hai,

We are using the MPC860 processor. we need the drivers for the processor. we need drivers for the SPI,UART and parellel interface can you please provide the drivers.(IDE code warrior 8.0  )

Thank you 

Best regards

Maheshwar.

0 Kudos
Reply
1 Reply

1,366 Views
Pavel
NXP Employee
NXP Employee

See simple program examples in the attached file.

If there is a problem for .zip or 7z file loading, create please technical case:

https://community.nxp.com/thread/381898


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply