DDR DRAM mode register address bits

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR DRAM mode register address bits

ソリューションへジャンプ
3,519件の閲覧回数
dallasclow
Contributor II

Are the bank address bits of the mode register settings (two msb's) of each field in DDR_SDRAM_MODE and DDR_SDRAM_MODE_2 used by the DDR controller at initialization or are they ignored?  There is a separate field for each specific mode register, which should allow the bank address bits to be ignored when addressing the DRAMs.  We're trying to assess the impact of a SW bug that incorrectly set the two msb's of the ESDMODE, ESDMODE2, and ESDMODE3 fields.  Would these to bits be ignored or cause incorrect DRAM mode register writes?

ラベル(1)
  • DDR

タグ(2)
0 件の賞賛
返信
1 解決策
3,461件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Would these to bits be ignored or cause incorrect DRAM mode register writes?

These bits are ignored.

元の投稿で解決策を見る

3 返答(返信)
3,461件の閲覧回数
dallasclow
Contributor II

This is an MPC8610.

0 件の賞賛
返信
3,462件の閲覧回数
ufedor
NXP Employee
NXP Employee

> Would these to bits be ignored or cause incorrect DRAM mode register writes?

These bits are ignored.

3,461件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which processor is in question?

0 件の賞賛
返信