DDR DRAM mode register address bits

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

DDR DRAM mode register address bits

跳至解决方案
2,366 次查看
dallasclow
Contributor II

Are the bank address bits of the mode register settings (two msb's) of each field in DDR_SDRAM_MODE and DDR_SDRAM_MODE_2 used by the DDR controller at initialization or are they ignored?  There is a separate field for each specific mode register, which should allow the bank address bits to be ignored when addressing the DRAMs.  We're trying to assess the impact of a SW bug that incorrectly set the two msb's of the ESDMODE, ESDMODE2, and ESDMODE3 fields.  Would these to bits be ignored or cause incorrect DRAM mode register writes?

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
2,308 次查看
ufedor
NXP Employee
NXP Employee

> Would these to bits be ignored or cause incorrect DRAM mode register writes?

These bits are ignored.

在原帖中查看解决方案

3 回复数
2,308 次查看
dallasclow
Contributor II

This is an MPC8610.

0 项奖励
回复
2,309 次查看
ufedor
NXP Employee
NXP Employee

> Would these to bits be ignored or cause incorrect DRAM mode register writes?

These bits are ignored.

2,308 次查看
ufedor
NXP Employee
NXP Employee

Which processor is in question?

0 项奖励
回复