Code-Worrier programming corruption with NOR flash in T2080RDB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Code-Worrier programming corruption with NOR flash in T2080RDB

ソリューションへジャンプ
2,757件の閲覧回数
singhawadhesh
Contributor I

Hi Team,

I was experimenting with NOR of T2080RDB and I have flashed U-boot with code-worrier in alternate bank of it. After making dump of that, I have compared it with actual file loaded into it with beyond compare (after converting both into HEX). I am finding there is mismatch in the dump data and the loaded file and unable to boot completely. When I am checking those locations (0xEBF4A19C) in memory window of debug, I am getting 0x4C00018C at every corrupted locations.

Please let me know the possible issue.

Thanks for your support.

Regards,

Awadhesh

0 件の賞賛
返信
1 解決策
2,740件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please upgrade to CodeWarrior 10.5.2 to check whether this problem could be resolved.

Please open CodeWarrior IDE, please click Help->Install New Software->Available Software Sites, please select "CodeWarrior Power Architecture v10.5.2 Release, click drop down list at "Work with", then select "CodeWarrior Power Architecture v10.5.2 Release - http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.updatesite_win/COMPILER", then install CodeWarrior 10.5.2 step by step.

 

元の投稿で解決策を見る

1 返信
2,741件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please upgrade to CodeWarrior 10.5.2 to check whether this problem could be resolved.

Please open CodeWarrior IDE, please click Help->Install New Software->Available Software Sites, please select "CodeWarrior Power Architecture v10.5.2 Release, click drop down list at "Work with", then select "CodeWarrior Power Architecture v10.5.2 Release - http://freescale.com/lgfiles/updates/Eclipse/PA10_5_1/com.freescale.pa.updatesite_win/COMPILER", then install CodeWarrior 10.5.2 step by step.