About fs65 design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About fs65 design

1,404 Views
StarMao159376
Contributor II

Hello, sir, the high level specification of the debug pin shows 4.35-4.97v, but the official recommendation is that vpre (6.5V) is divided by 10k/11k resistors in the circuit. After calculation, the actual high level is about 3.25V, which can not meet the high level range of 4.35-4.97v defined by this pin. What is the final design subject to?

StarMao159376_0-1655301047196.jpegStarMao159376_1-1655301066476.jpeg

 

Labels (1)
0 Kudos
Reply
0 Replies