About BDM debug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About BDM debug

1,426件の閲覧回数
tomlucas
Contributor II

For protection, what tricks can be used for prohibitting bdm debug in mpc8xx processor?

1 返信

1,330件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

BDM interface can not be protected in MPC8xx - there is no "debug disable" fuses or something like that.

So, there is no 100% guarantied way to protect your MPC8xx device from debugging, but:

1. You can reconfigure debug port pins to other functions in DBGC / DBPC fields of RCW

2. In your software you can detect the fact that the debug mode is enabled and behave differently, for example erase critical data.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------