About BDM debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About BDM debug

1,446 Views
tomlucas
Contributor II

For protection, what tricks can be used for prohibitting bdm debug in mpc8xx processor?

1 Reply

1,350 Views
alexander_yakov
NXP Employee
NXP Employee

BDM interface can not be protected in MPC8xx - there is no "debug disable" fuses or something like that.

So, there is no 100% guarantied way to protect your MPC8xx device from debugging, but:

1. You can reconfigure debug port pins to other functions in DBGC / DBPC fields of RCW

2. In your software you can detect the fact that the debug mode is enabled and behave differently, for example erase critical data.


Have a great day,
Alexander

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------