mc33771 i2c

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

mc33771 i2c

跳至解决方案
2,241 次查看
jesus_hernandez
Contributor I

Hello, I am evaluating the mc33771 battery cell manager ic for use in a bms design I'm working on. I was wondering if there was any documentation regarding using the I2C pins on the mc33771 to communicate to another device? I do not require the eeprom chip on the evaluation board. I'd like to expose those pins so I could attach some sensors.

标记 (1)
0 项奖励
回复
1 解答
2,180 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jesus,

The I2C interface on the MC33771 is intended to be used only with an external EEPROM to store calibration parameters defined by the user. It does not allow interfacing other ICs such as sensors etc.

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,181 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jesus,

The I2C interface on the MC33771 is intended to be used only with an external EEPROM to store calibration parameters defined by the user. It does not allow interfacing other ICs such as sensors etc.

Best regards,

Tomas

0 项奖励
回复