mc33771 i2c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,253件の閲覧回数
jesus_hernandez
Contributor I

Hello, I am evaluating the mc33771 battery cell manager ic for use in a bms design I'm working on. I was wondering if there was any documentation regarding using the I2C pins on the mc33771 to communicate to another device? I do not require the eeprom chip on the evaluation board. I'd like to expose those pins so I could attach some sensors.

タグ(1)
0 件の賞賛
返信
1 解決策
2,192件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jesus,

The I2C interface on the MC33771 is intended to be used only with an external EEPROM to store calibration parameters defined by the user. It does not allow interfacing other ICs such as sensors etc.

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,193件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jesus,

The I2C interface on the MC33771 is intended to be used only with an external EEPROM to store calibration parameters defined by the user. It does not allow interfacing other ICs such as sensors etc.

Best regards,

Tomas

0 件の賞賛
返信