XS2410 - Current and Voltage Accuracy Clarification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XS2410 - Current and Voltage Accuracy Clarification

Jump to solution
1,607 Views
adamrosy
Contributor I

I have a question regarding the stated current and voltage measurement accuracy for the XS2410.

Am I correct in understanding that the measurement accuracy increases with increasing current? Reading the graph, an output current of 50mA, I would expect the measurement to be within 30% of actual, and at 1A the accuracy would be within ~8% of actual?

adamrosy_0-1747217547786.png

I cannot find any information about the range values for the stated "low" and "high" current ranges so that would also be useful to know if the accuracy changes in either of these ranges, or if the graph can be used to determine the accuracy.

Thank you!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,595 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Adam,

Yes, the current measurement accuracy does improve with increasing load current. At very low currents (e.g. 5mA), the error is high, so those measurements are useful mainly for detecting presence or absence (e.g. open load), not for precision. At mid-range current (e.g. 200mA), the error drops significantly, but is still not ideal for precise monitoring. Once you reach 1A or more, the current measurement is much more reliable and within ±6%.

Snímek obrazovky 2025-05-14 142816.png

BRs, Tomas

View solution in original post

2 Replies
1,576 Views
adamrosy
Contributor I

Hi Tomas,

Brilliant, thank you confirming that!

Best regards,
Adam

0 Kudos
Reply
1,596 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Adam,

Yes, the current measurement accuracy does improve with increasing load current. At very low currents (e.g. 5mA), the error is high, so those measurements are useful mainly for detecting presence or absence (e.g. open load), not for precision. At mid-range current (e.g. 200mA), the error drops significantly, but is still not ideal for precise monitoring. Once you reach 1A or more, the current measurement is much more reliable and within ±6%.

Snímek obrazovky 2025-05-14 142816.png

BRs, Tomas