Whether FS6523 assert FS0B low when a external reset detected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Whether FS6523 assert FS0B low when a external reset detected

ソリューションへジャンプ
3,092件の閲覧回数
Jamber_H
Contributor III

During FS6523 running normally in debug mode, an external reset is assert by MCU, whether FS6523 assert FS0B low in this condition?

In user manual Fail Safe Machine, external reset will set the SBC to Release RST phase, in the picture, it said FSxB assert low, is it means FS6523 will assert FS0B low if an external reset occured?

2021-09-24_140928.png2021-09-24_140928.png

Best Regards

Jamber

0 件の賞賛
返信
1 解決策
3,075件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jamber,

please refer to section 11.16 in the FS45/FS65 datasheet. The behavior of the FS0B and FS1B outputs in debug mode are the same as in normal mode. So the answer is yes. FS0B will be low if the external reset occurs.

JozefKozon_0-1632723461901.pngJozefKozon_0-1632723461901.png

With Best Regards,

Jozef

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,076件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jamber,

please refer to section 11.16 in the FS45/FS65 datasheet. The behavior of the FS0B and FS1B outputs in debug mode are the same as in normal mode. So the answer is yes. FS0B will be low if the external reset occurs.

JozefKozon_0-1632723461901.pngJozefKozon_0-1632723461901.png

With Best Regards,

Jozef

0 件の賞賛
返信