Whether FS6523 assert FS0B low when a external reset detected

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Whether FS6523 assert FS0B low when a external reset detected

跳至解决方案
2,483 次查看
Jamber_H
Contributor III

During FS6523 running normally in debug mode, an external reset is assert by MCU, whether FS6523 assert FS0B low in this condition?

In user manual Fail Safe Machine, external reset will set the SBC to Release RST phase, in the picture, it said FSxB assert low, is it means FS6523 will assert FS0B low if an external reset occured?

2021-09-24_140928.png

Best Regards

Jamber

0 项奖励
回复
1 解答
2,466 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jamber,

please refer to section 11.16 in the FS45/FS65 datasheet. The behavior of the FS0B and FS1B outputs in debug mode are the same as in normal mode. So the answer is yes. FS0B will be low if the external reset occurs.

JozefKozon_0-1632723461901.png

With Best Regards,

Jozef

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,467 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Jamber,

please refer to section 11.16 in the FS45/FS65 datasheet. The behavior of the FS0B and FS1B outputs in debug mode are the same as in normal mode. So the answer is yes. FS0B will be low if the external reset occurs.

JozefKozon_0-1632723461901.png

With Best Regards,

Jozef

0 项奖励
回复