Wake up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Wake up

2,382件の閲覧回数
Wen666
Contributor II

Hello, I have a question about the FS6500 wake-up configuration. After the wake up event is detected, according to the FS6500 data document, the master state machine does not need to be re-initialized while the fail-safe state machine needs to be re-initialized. I would like to ask if there is a register configuration process for post-wake initialization, similar to Figure 2.

屏幕截图 2024-09-25 152532.png屏幕截图 2024-09-25 152532.png

屏幕截图 2024-09-25 150016.png屏幕截图 2024-09-25 150016.png

  

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,364件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

You can re-write the INIT related registers to enter into normal mode,but INIT_INT register MUST be operated.

0 件の賞賛
返信

2,348件の閲覧回数
Wen666
Contributor II

I wonder what the nest software needs to do in order to wake up from sleep mode to normal mode, is it the same logic as reset power on or is it just a matter of configuring the relevant registers of the fail-safe state machine.

タグ(1)
0 件の賞賛
返信

2,249件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

You can see below,from wake up the MAIN STATE MACHINE ,will enter into Buck or
Buck Boost configuration detection phase and Keep going down according the arrow flow.

guoweisun_1-1729048274297.pngguoweisun_1-1729048274297.png

 

 

0 件の賞賛
返信