Wake up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Wake up

2,390 Views
Wen666
Contributor II

Hello, I have a question about the FS6500 wake-up configuration. After the wake up event is detected, according to the FS6500 data document, the master state machine does not need to be re-initialized while the fail-safe state machine needs to be re-initialized. I would like to ask if there is a register configuration process for post-wake initialization, similar to Figure 2.

屏幕截图 2024-09-25 152532.png屏幕截图 2024-09-25 152532.png

屏幕截图 2024-09-25 150016.png屏幕截图 2024-09-25 150016.png

  

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,372 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

You can re-write the INIT related registers to enter into normal mode,but INIT_INT register MUST be operated.

0 Kudos
Reply

2,356 Views
Wen666
Contributor II

I wonder what the nest software needs to do in order to wake up from sleep mode to normal mode, is it the same logic as reset power on or is it just a matter of configuring the relevant registers of the fail-safe state machine.

Tags (1)
0 Kudos
Reply

2,257 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can see below,from wake up the MAIN STATE MACHINE ,will enter into Buck or
Buck Boost configuration detection phase and Keep going down according the arrow flow.

guoweisun_1-1729048274297.pngguoweisun_1-1729048274297.png

 

 

0 Kudos
Reply