Vsense in MC33FS4503

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
7,059件の閲覧回数
jingfang
Contributor IV

Data sheet: Vsense must be connected to the battery line(before the reverse battery protection diode),but the PCB is recommends to be connected behind the diode.

We originally designed Power A,but now we want to add Power B. We want to move the node to the positon of the red arrow. Will this have any impact?

0 件の賞賛
返信
1 解決策
7,054件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jingfang,

Both connections are OK from a functional safety point of view since VSENSE is rated -14 to 40V (with ext R in series mandatory) and is also the redundant supply for the Fail-safe machine (primary supply is VSUP3).

Having said that, we recommend to connect the VSENSE pin before the reverse protection diode. This allows to have the real image of the battery voltage for the sensing (for the AMUX for instance), avoiding the drop in the diode.

Best regards,

Tomas



元の投稿で解決策を見る

1 返信
7,055件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Jingfang,

Both connections are OK from a functional safety point of view since VSENSE is rated -14 to 40V (with ext R in series mandatory) and is also the redundant supply for the Fail-safe machine (primary supply is VSUP3).

Having said that, we recommend to connect the VSENSE pin before the reverse protection diode. This allows to have the real image of the battery voltage for the sensing (for the AMUX for instance), avoiding the drop in the diode.

Best regards,

Tomas