VR5510 test mode also at pre-programmed devices

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VR5510 test mode also at pre-programmed devices

ソリューションへジャンプ
1,880件の閲覧回数
K_Steinhammer
Contributor III

The documentation of the VR5510 is not clear at this point:

Is it possible to continue entering test mode or debug mode with an already programmed device in order to continue testing of parameter sets like it is possible with an un-programmed (empty) device?

Thanks

  Klaus

 

PS: I know that I can program the device only once, but I want to know if I can continue to use an already programmed device for further optimizing the parameter set during development testing.

0 件の賞賛
返信
1 解決策
1,873件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Klaus,

I hope all is great with you.

You are correct, you will be able to enter in Debug mode even with a programmed device. You may follow the procedure mentioned on datasheet, chapter 8.12.

I hope this information helps.

Regards,

David

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,874件の閲覧回数
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Klaus,

I hope all is great with you.

You are correct, you will be able to enter in Debug mode even with a programmed device. You may follow the procedure mentioned on datasheet, chapter 8.12.

I hope this information helps.

Regards,

David

0 件の賞賛
返信