VR5510 Power-On & Power-Off issue repeatly

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VR5510 Power-On & Power-Off issue repeatly

820 Views
Jerry87
Contributor I

Hello Sir, 

My design is based on NXP’s GoldBox. The only difference is that GoldBox pow-rail  is +12V DC, but my design is +14.4V DC as shown in picture below.

However, on my prototypes, we have seen the fact that VPRE_3V3 (IC Pins: 35, 36, 6) is power ON, power OFF, power ON, power OFF etc repeatedly. 

My finding:

  1. When we removed C477, this issue can be resolved. So we suspect that there is a timing issue on power on sequence on PWRON1.
  2. In GoldBox, PWRON1 take 5.12ms for rising edge in average; our design is about 7ms for rising edge in average. Could you please let us know what the minimum & maximum rising edge time of PWRON1?
  3. Based on our issue, is there any other points that we need to investigate?

 

Jerry87_1-1668638405229.png

 

Jerry87_0-1668638393610.png

 

0 Kudos
Reply
1 Reply

807 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello Jerry,

I hope all is great with you.

Please review the response from the PMICs team below:

diazmarin09_0-1668784141714.png

 

Please check below plot, we recommend T1>3ms,  T2>7ms. Customer can check whether the T2>7ms is met.  

Therefore, to power up PWRON12 should wait at least 3ms. Once it is powered up, you should maintain VDDOTP at least 7ms more.

I hope this information helps.

Regards,

0 Kudos
Reply