UJA1169 wake-up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UJA1169 wake-up

Jump to solution
2,199 Views
Tracy_Lu
Contributor II

Hi,dear NXP colleague:

UJA1169,after wake-up in sleep mode,  V1 will rise up,may I ask the delay time between these two event?many,many,many thanks !!![rose][rose]

0 Kudos
Reply
1 Solution
2,185 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Tracy,

When the SBC wakes up from Sleep mode, it transitions through Reset mode and then to Standby mode, at which point the V1 regulator is enabled to supply the microcontroller.

According to the datasheet (Section 11 – Dynamic Characteristics), the delay for V1 to reach 90% of its nominal voltage is defined as the start-up time (Tstartup).

The specified values are:
Typical: 2.8ms
Maximum: 4.7ms

So, after a wake-up event in Sleep mode, V1 will typically be available within approximately 3–5ms.

BRs, Tomas

View solution in original post

0 Kudos
Reply
2 Replies
2,186 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Tracy,

When the SBC wakes up from Sleep mode, it transitions through Reset mode and then to Standby mode, at which point the V1 regulator is enabled to supply the microcontroller.

According to the datasheet (Section 11 – Dynamic Characteristics), the delay for V1 to reach 90% of its nominal voltage is defined as the start-up time (Tstartup).

The specified values are:
Typical: 2.8ms
Maximum: 4.7ms

So, after a wake-up event in Sleep mode, V1 will typically be available within approximately 3–5ms.

BRs, Tomas

0 Kudos
Reply
2,168 Views
Tracy_Lu
Contributor II

Got it!the explanation is explicit and professional !!

thanks,Tomas!

0 Kudos
Reply