TEA2208

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,006件の閲覧回数
alessandrocunha
Contributor I

Any usage example available for this TEA2208 that I can share with my customers?

0 件の賞賛
返信
1 解決策
2,996件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Alessandro,

 

The TEA2208T is intended for power supplies with a boost-type power-factor controller as a first stage. The second stage can be a resonant controller, a flyback controller, or any other controller topology. It can be used in all power supplies requiring high efficiency:

  • (Notebook) Adapters
  • Power supplies for desktop and all-in-one PCs
  • Power supplies for gaming consoles
  • Power supplies for UHD LED / OLED televisions
  • Power supplies for servers / 5G

 

Currently we offer the TEA2208DB1576 demo board. In the UM11348 (Fig. 5) you can see this board mounted on the TEA2016DB1519 240W resonant adapter board.

 

Best regards,

Tomas

元の投稿で解決策を見る

2 返答(返信)
2,997件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Alessandro,

 

The TEA2208T is intended for power supplies with a boost-type power-factor controller as a first stage. The second stage can be a resonant controller, a flyback controller, or any other controller topology. It can be used in all power supplies requiring high efficiency:

  • (Notebook) Adapters
  • Power supplies for desktop and all-in-one PCs
  • Power supplies for gaming consoles
  • Power supplies for UHD LED / OLED televisions
  • Power supplies for servers / 5G

 

Currently we offer the TEA2208DB1576 demo board. In the UM11348 (Fig. 5) you can see this board mounted on the TEA2016DB1519 240W resonant adapter board.

 

Best regards,

Tomas

2,984件の閲覧回数
alessandrocunha
Contributor I

Thank you @TomasVaverka !

 

Exactly this that I need!

 

Regards

0 件の賞賛
返信