PF1550 supplied from an external source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF1550 supplied from an external source

Jump to solution
2,021 Views
Davide91
Contributor I

Hello,

There is something I cannot understand from PF1550 datasheet: can the PMIC be supplied from an external source, even if the battery is present and being loaded?

How does the VSYS voltage interact with the battery charge? Is it possible to provide VSYS from an external source?

Thanks

Davide

0 Kudos
Reply
1 Solution
2,011 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Davide,

 

Yes, the PMIC be supplied from an external source, even if the battery is present and being loaded, use external 5.0V from USB on VBUSIN.

 

VSYS voltage interact with the battery charge. VSYSMIN parameter sets the point where the VSYS loop starts taking control and regulates the output. 4.3 V is the recommended setting to ensure that there is enough headroom before reaching UVDET.

Check Figure 17 of the datasheet that shows the charging profile for a better understanding of the relationship between VSYS and the battery charge.

 

Do not connect external source to VSYS.

 

Regards,

Jose

View solution in original post

0 Kudos
Reply
1 Reply
2,012 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Davide,

 

Yes, the PMIC be supplied from an external source, even if the battery is present and being loaded, use external 5.0V from USB on VBUSIN.

 

VSYS voltage interact with the battery charge. VSYSMIN parameter sets the point where the VSYS loop starts taking control and regulates the output. 4.3 V is the recommended setting to ensure that there is enough headroom before reaching UVDET.

Check Figure 17 of the datasheet that shows the charging profile for a better understanding of the relationship between VSYS and the battery charge.

 

Do not connect external source to VSYS.

 

Regards,

Jose

0 Kudos
Reply