Supplying power using PMIC for i.MX 6ULZ reference design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Supplying power using PMIC for i.MX 6ULZ reference design

ソリューションへジャンプ
4,570件の閲覧回数
oscar_duran
Contributor I

Where do I find a reference design that uses PMIC for i.MX 6ULZ?

ラベル(4)
1 解決策
4,298件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Oscar,

6ULZ is same silicon as 6ULL, therefore we propose the PF1550.

PF1550: https://www.nxp.com/products/power-management/pmics/pmics-for-i.mx-application-processors/pmic-with-...

 

We have a schematic that you can use as a HW reference design, see the below PF1550 + i.MX 6ULL reference design, and enclosed schematic in PDF format.

 

KIT6ULL-1550EVM (PF1550 + i.MX6ULL).

SCH-29464,1.35V LvDDR3

 

Please let me know if you need more information.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
1,860件の閲覧回数
ET_Dev
Contributor III

Hello

Is it possible to share the hardware design files for the KIT6ULL-1550EVM as well? 

0 件の賞賛
返信
4,299件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi Oscar,

6ULZ is same silicon as 6ULL, therefore we propose the PF1550.

PF1550: https://www.nxp.com/products/power-management/pmics/pmics-for-i.mx-application-processors/pmic-with-...

 

We have a schematic that you can use as a HW reference design, see the below PF1550 + i.MX 6ULL reference design, and enclosed schematic in PDF format.

 

KIT6ULL-1550EVM (PF1550 + i.MX6ULL).

SCH-29464,1.35V LvDDR3

 

Please let me know if you need more information.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

4,298件の閲覧回数
oscar_duran
Contributor I

Hi Jose,

Thank you fot you answer, an apologise for thed delay.

Effectivelly, the RD that you recomend was very usefull for me.

Have a great day to.

0 件の賞賛
返信