We are developing a board with RT1175 and MPF5020CMMACES.
Where can I find a reference design schematic, or some docs?
Please note that I read AN13213, but there is only the PMIC portion of the schematic there, I also need the reference design for RT1175.
I am convinced that NXP had to develop a board to test MPF5020 with RT117x. I wish I could see the schematics of that board.
best regards
Max
Thank you, this is really helpful to me.
Is this board also available for purchase?
best regards
Dear Massimiliano,
yes, there is the board available. But not the rev. A, to which I have shared the schematic, but a newer rev. C1. The board name is: MIMXRT1170-EVKB. Please refer to the Revision History in the SPF-55139_c1 schematic attached.
With Best Regards,
Jozef