Power Supply for LS1046

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Power Supply for LS1046

5,518 Views
Ellu24
Contributor III

I am trying to bring up a board using LS1046 and using a design similar to freeway board. I am using PF8100 and LTC7150 for multioutput voltages and VDD respectively. I am using programmable DC power supply for giving 3.3V,3 A and 12V,1.8A as input and not observing the expected voltages. Please find the attachment to see the measured and expected voltages. Please help me to resolve the problem.

Is there any software to simulate PF8100?

 

Thanks in advance 

0 Kudos
Reply
5 Replies

5,500 Views
Ellu24
Contributor III

Thank you very much for your advice.

I will do as per your recommendations and let you know the outcome. Is there any software that we can simulate PF8100 and observe the waveforms? Is there any reason for the unexpected voltages?

 

Thanks in advance 

0 Kudos
Reply

5,492 Views
guoweisun
NXP TechSupport
NXP TechSupport

No more the simulation model for this part.

Lots of reasons can lead to the error output,for example mistake on mount components/mistake for select regulator components/etcs.

0 Kudos
Reply

5,511 Views
Ellu24
Contributor III

Thank you very much for your prompt response. I am testing the power supply with the complete board, so that I hope each channel has load. Or please recommend me on adding load on each channel.

0 Kudos
Reply

5,510 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can try to add external 500mA on such as 2.5V output channel, then test again.

0 Kudos
Reply

5,513 Views
guoweisun
NXP TechSupport
NXP TechSupport

Did you add the load on each channel? If not please add load to test again.

 

0 Kudos
Reply