Piezo fuel DI injector Driver?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Piezo fuel DI injector Driver?

7,078 Views
mabroglia2
Contributor II

Hello

I would like know with NXP experts if NPX has any solution(IC, application note, circuit, ...) to drive Piezo Injector of Direct Injection for Gasoline Internal Combustion engine?

My intention is develop a driver circuit for a stand alone tester for DI Fuel Injectors with Piezo Architecture.

Note:

I saw PT2000 IC, is very interesting IC, but in my opinion can't drive a Piezo Injector more than 72V.

Best Regards.

Marco Broglia.

Labels (1)
Tags (2)
0 Kudos
Reply
6 Replies

6,945 Views
mabroglia2
Contributor II

Helio G. W. Sun.

No, according PT2000 datasheet:

VBOOST <=72V.

Piezoelectric Injector needs 120V to activate piezo elements and probably more than 8A(depends the number of piezo elements, and capacitance of each element), PT2000 is not enough to drive Peizo Injectors.

Probably I need a DCDC boost that store more than 900W, and internal feedback to IC must read more than 120V.

If someone has a proposal to solve this problem, I am happy to know.

Best Regards

Marco Broglia

6,841 Views
Jooin
Contributor I

Hello
I'm in the same problem.
I'm studying the control algorithm for piezo injectors in college. I found a good IC, PT2000, but it cannot be used due to the conditions of Vboost <=72. I have to meet Vboost conditions above 120V.
Did you find any suitable solution?
If possible, could you share it with me?

Best Regards

Jooin Lee

0 Kudos
Reply

6,945 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi Marco

Thanks for your update! That's interesting request!

Can you give us your project information more here?

1: company name

2:end products

3:volume/annual

4:project schedule

6,945 Views
mabroglia2
Contributor II

In private?

6,945 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please send to-   [email protected]

6,945 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

Do you mean the battery voltage input up to 72V support?

0 Kudos
Reply