RESET AND WATCHDOG PARAMETERS - FS6500

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RESET AND WATCHDOG PARAMETERS - FS6500

跳至解决方案
2,601 次查看
AnneVilasini
Contributor I

Hi , 

What is the maximum time taken for a reset to occur when a fault has occured? (indicated by Trr in the picture below)?

AnneVilasini_0-1606968849523.png

 

 

标签 (1)
0 项奖励
回复
1 解答
2,593 次查看
guoweisun
NXP TechSupport
NXP TechSupport

There is some misunderstanding for the reaction time and  Trr. To make clear, I will describe the total process for a fault happen and Reset assertion:

1. Recognition time

When output voltage reach UV threshold, and the duration time of output<UV Threshold larger than 10uS(max value),UV event will be recognized. It is 234us for an overvoltage recognition.

2. Internal Processing Time

After an fault recognized, it will take some time for internal Processing, the longest time is about 80 μs for an overvoltage detection. All others are below 80 μs.

3. External indication time 

External indication time to notify an observer about the failure external to the SBC. This time is 3.0 µs for RSTB, 22 μs for FS0B .

 

so,

It should be 10uS+80uS+3uS=93uS(max) from an undervoltage happen to RSTB asserted to Low;

it should be 234uS+80uS+3uS=317uS(max) from an overvoltage happen to RSTB asserted to Low; 

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,594 次查看
guoweisun
NXP TechSupport
NXP TechSupport

There is some misunderstanding for the reaction time and  Trr. To make clear, I will describe the total process for a fault happen and Reset assertion:

1. Recognition time

When output voltage reach UV threshold, and the duration time of output<UV Threshold larger than 10uS(max value),UV event will be recognized. It is 234us for an overvoltage recognition.

2. Internal Processing Time

After an fault recognized, it will take some time for internal Processing, the longest time is about 80 μs for an overvoltage detection. All others are below 80 μs.

3. External indication time 

External indication time to notify an observer about the failure external to the SBC. This time is 3.0 µs for RSTB, 22 μs for FS0B .

 

so,

It should be 10uS+80uS+3uS=93uS(max) from an undervoltage happen to RSTB asserted to Low;

it should be 234uS+80uS+3uS=317uS(max) from an overvoltage happen to RSTB asserted to Low; 

 

0 项奖励
回复