FS6500 - INTERNAL RESET CIRCUITRY

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FS6500 - INTERNAL RESET CIRCUITRY

1,951件の閲覧回数
AnneVilasini
Contributor I

Hi ,

My query is regarding the internal reset circuitry used in SBC FS6500.

1. What is the maximum reaction time Trr of the reset ?

2. What is the maximum voltage drop that can occur during Trr max ?(indicated by delta U in the picture)

3.What is the minimum threshold voltage Vrt, which triggers a reset from the reset circuitry? (indicated by Vrt min in the picture)

4. What is the minimum voltage Vdd, which ensures the ECU does not reset?

AnneVilasini_0-1606796992538.png

 

0 件の賞賛
返信
2 返答(返信)

1,945件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

1. What is the maximum reaction time Trr of the reset ?

overvoltage is the maximum reaction time 83uS;

2. What is the maximum voltage drop that can occur during Trr max ?(indicated by delta U in the picture)

It depends on output capacitor and loads after regulators.

3.What is the minimum threshold voltage Vrt, which triggers a reset from the reset circuitry? (indicated by Vrt min in the picture)

If UV configured as RSTB impacted, it is min UV threshold that can be found in the datasheet

4. What is the minimum voltage Vdd, which ensures the ECU does not reset?

it corresponding to the max UV threshold that can be found in the datasheet.

0 件の賞賛
返信

1,935件の閲覧回数
AnneVilasini
Contributor I

Hi Guoweisen, 

Thanks for your reply, 

Could you also please let me know , how the maximum reaction time of reset is considered as 83us?

 

0 件の賞賛
返信