Piezo fuel DI injector Driver?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Piezo fuel DI injector Driver?

7,069件の閲覧回数
mabroglia2
Contributor II

Hello

I would like know with NXP experts if NPX has any solution(IC, application note, circuit, ...) to drive Piezo Injector of Direct Injection for Gasoline Internal Combustion engine?

My intention is develop a driver circuit for a stand alone tester for DI Fuel Injectors with Piezo Architecture.

Note:

I saw PT2000 IC, is very interesting IC, but in my opinion can't drive a Piezo Injector more than 72V.

Best Regards.

Marco Broglia.

ラベル(1)
タグ(2)
0 件の賞賛
返信
6 返答(返信)

6,936件の閲覧回数
mabroglia2
Contributor II

Helio G. W. Sun.

No, according PT2000 datasheet:

VBOOST <=72V.

Piezoelectric Injector needs 120V to activate piezo elements and probably more than 8A(depends the number of piezo elements, and capacitance of each element), PT2000 is not enough to drive Peizo Injectors.

Probably I need a DCDC boost that store more than 900W, and internal feedback to IC must read more than 120V.

If someone has a proposal to solve this problem, I am happy to know.

Best Regards

Marco Broglia

6,832件の閲覧回数
Jooin
Contributor I

Hello
I'm in the same problem.
I'm studying the control algorithm for piezo injectors in college. I found a good IC, PT2000, but it cannot be used due to the conditions of Vboost <=72. I have to meet Vboost conditions above 120V.
Did you find any suitable solution?
If possible, could you share it with me?

Best Regards

Jooin Lee

0 件の賞賛
返信

6,936件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi Marco

Thanks for your update! That's interesting request!

Can you give us your project information more here?

1: company name

2:end products

3:volume/annual

4:project schedule

6,936件の閲覧回数
mabroglia2
Contributor II

In private?

6,936件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please send to-   [email protected]

6,936件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

HI

Do you mean the battery voltage input up to 72V support?

0 件の賞賛
返信