PF8200 open drain pull up voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF8200 open drain pull up voltage

ソリューションへジャンプ
2,751件の閲覧回数
adevries
Contributor V

Hello,

I am working on a design that uses the PF8200. RESETB_MCU, INTB, PGOOD, and FSOB are all open drain signals that the datasheet recommends pulling up to VDDIO. However, for my application, I would like to pull them to a slightly different voltage. Since these are all open drain outputs, I believe this is acceptable, but I was hoping someone from NXP could provide a little more direction. Here are my questions:

1. Does the voltage on VDDIO affect how high I can pull the open drain outputs? For example, if VDDIO is 1.8V, can I pull the open drain outputs to 3.3V and still get proper operation?

2. If VDDIO is 3.3V, can I pull the open drain outputs to 1.8V and still have them work properly?

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
2,630件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

HI

Please see comment:

1. Does the voltage on VDDIO affect how high I can pull the open drain outputs? For example, if VDDIO is 1.8V, can I pull the open drain outputs to 3.3V and still get proper operation?

[gw]Yes,you can!

2. If VDDIO is 3.3V, can I pull the open drain outputs to 1.8V and still have them work properly?

[gw]Yes,you can!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,631件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

HI

Please see comment:

1. Does the voltage on VDDIO affect how high I can pull the open drain outputs? For example, if VDDIO is 1.8V, can I pull the open drain outputs to 3.3V and still get proper operation?

[gw]Yes,you can!

2. If VDDIO is 3.3V, can I pull the open drain outputs to 1.8V and still have them work properly?

[gw]Yes,you can!

0 件の賞賛
返信