FS8430 can not wake up

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS8430 can not wake up

2,196 Views
hongyuyan
Contributor I

Hi NXP Team,

I have a problem about FS8430.

when I give the BAT and wake signal to FS8430 at the same time,it can start up normally at the voltage from 8V ~ 36V.But when I  give the BAT at 9V first and then wake signal, FS8430 can not start up normally. At this condition, beside 8v~10V, FS8430 can start up normally.

I want to know what is the main reason.

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

2,045 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

Suggest your do experiment on debug mode then monitor your Vbat voltage directly in SBC VSUP1/2 pin and WAKE pins voltge.

0 Kudos
Reply