PF8200 VIN vs SWXIN Voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF8200 VIN vs SWXIN Voltage

Jump to solution
4,333 Views
adevries
Contributor V

Hello,

For the PF8200, is it important to have the voltage on VIN match the voltage on the Switch and LDO inputs? (SW1IN-SW7IN and LDO12IN-LDO4IN). Or can VIN be run at 3.3V while the Switch and LDO inputs are at 5V?

Thanks

Labels (3)
1 Solution
4,136 Views
nelson_scheja
Contributor III

I just created a thread about exactly this topic few days ago: Different inpult voltages lead to destruction??? 

So, despite the datasheet saying nothing about it, this is not allowed.

View solution in original post

4 Replies
4,136 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Don't suggest your do that! Using VIN different from SW and LDO input.

4,136 Views
adevries
Contributor V

Hi G.W. Sun,

Thanks for the response. Would it be safe for me to have VIN at 5V, and SW and LDO inputs unpowered (at 0V)? Or will that also break the PF8200?

0 Kudos
Reply
4,137 Views
nelson_scheja
Contributor III

I just created a thread about exactly this topic few days ago: Different inpult voltages lead to destruction??? 

So, despite the datasheet saying nothing about it, this is not allowed.

4,136 Views
adevries
Contributor V

Oh wow, thank you for linking that thread. I'm really glad I asked this question. Thanks for the info!

0 Kudos
Reply