PF8200 VIN vs SWXIN Voltage

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PF8200 VIN vs SWXIN Voltage

跳至解决方案
4,344 次查看
adevries
Contributor V

Hello,

For the PF8200, is it important to have the voltage on VIN match the voltage on the Switch and LDO inputs? (SW1IN-SW7IN and LDO12IN-LDO4IN). Or can VIN be run at 3.3V while the Switch and LDO inputs are at 5V?

Thanks

标签 (3)
标记 (3)
1 解答
4,147 次查看
nelson_scheja
Contributor III

I just created a thread about exactly this topic few days ago: Different inpult voltages lead to destruction??? 

So, despite the datasheet saying nothing about it, this is not allowed.

在原帖中查看解决方案

4 回复数
4,147 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Don't suggest your do that! Using VIN different from SW and LDO input.

4,147 次查看
adevries
Contributor V

Hi G.W. Sun,

Thanks for the response. Would it be safe for me to have VIN at 5V, and SW and LDO inputs unpowered (at 0V)? Or will that also break the PF8200?

0 项奖励
回复
4,148 次查看
nelson_scheja
Contributor III

I just created a thread about exactly this topic few days ago: Different inpult voltages lead to destruction??? 

So, despite the datasheet saying nothing about it, this is not allowed.

4,147 次查看
adevries
Contributor V

Oh wow, thank you for linking that thread. I'm really glad I asked this question. Thanks for the info!

0 项奖励
回复