PF8200 OTP Programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF8200 OTP Programming

ソリューションへジャンプ
4,163件の閲覧回数
adevries
Contributor V

Hello,

I'm interested in programming the OTP bits in the PF8200. I saw that it can be done via I2C, but I cannot find an OTP programming specification document for it, and the datasheet says to contact NXP. So how do I accomplish programming the OTP memory in the PF8200?

Thanks

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
3,936件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

We have a programming adapter for it:  PF8200/PF8100 Programming Board | NXP 

This works together with the FlexGUI software.

If you have un-programmed PF8200 samples, then you can use this tool to program the OTP.

The Configuration Reports for our standard types on this site  

      PMIC for high-performance applications | NXP 

can be used as a guideline for the values you typically need to apply to the FlexGUI software, in order to generate an OTP programming file:

For production purposes, we recommend to use a partner, who can program and test them before they get assembled.

Regards,

Bernhard.

元の投稿で解決策を見る

3 返答(返信)
3,936件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

We don't recommend to you do OTP by yourself,you can contact with you local NXP distributors for applying

OTP request then you will get your desire OTP parts.

0 件の賞賛
返信
3,937件の閲覧回数
bernhardfink
NXP Employee
NXP Employee

We have a programming adapter for it:  PF8200/PF8100 Programming Board | NXP 

This works together with the FlexGUI software.

If you have un-programmed PF8200 samples, then you can use this tool to program the OTP.

The Configuration Reports for our standard types on this site  

      PMIC for high-performance applications | NXP 

can be used as a guideline for the values you typically need to apply to the FlexGUI software, in order to generate an OTP programming file:

For production purposes, we recommend to use a partner, who can program and test them before they get assembled.

Regards,

Bernhard.

3,936件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Thanks!

0 件の賞賛
返信