PF8200 OTP Programming

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF8200 OTP Programming

Jump to solution
4,343 Views
adevries
Contributor V

Hello,

I'm interested in programming the OTP bits in the PF8200. I saw that it can be done via I2C, but I cannot find an OTP programming specification document for it, and the datasheet says to contact NXP. So how do I accomplish programming the OTP memory in the PF8200?

Thanks

Labels (2)
0 Kudos
Reply
1 Solution
4,116 Views
bernhardfink
NXP Employee
NXP Employee

We have a programming adapter for it:  PF8200/PF8100 Programming Board | NXP 

This works together with the FlexGUI software.

If you have un-programmed PF8200 samples, then you can use this tool to program the OTP.

The Configuration Reports for our standard types on this site  

      PMIC for high-performance applications | NXP 

can be used as a guideline for the values you typically need to apply to the FlexGUI software, in order to generate an OTP programming file:

For production purposes, we recommend to use a partner, who can program and test them before they get assembled.

Regards,

Bernhard.

View solution in original post

3 Replies
4,116 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi

We don't recommend to you do OTP by yourself,you can contact with you local NXP distributors for applying

OTP request then you will get your desire OTP parts.

0 Kudos
Reply
4,117 Views
bernhardfink
NXP Employee
NXP Employee

We have a programming adapter for it:  PF8200/PF8100 Programming Board | NXP 

This works together with the FlexGUI software.

If you have un-programmed PF8200 samples, then you can use this tool to program the OTP.

The Configuration Reports for our standard types on this site  

      PMIC for high-performance applications | NXP 

can be used as a guideline for the values you typically need to apply to the FlexGUI software, in order to generate an OTP programming file:

For production purposes, we recommend to use a partner, who can program and test them before they get assembled.

Regards,

Bernhard.

4,116 Views
guoweisun
NXP TechSupport
NXP TechSupport

Thanks!

0 Kudos
Reply