PF8100CCES Feasibility

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PF8100CCES Feasibility

跳至解决方案
3,279 次查看
deega_jung
Contributor III

Hi,

Target AP : MIMX8QX1AVLFZAC

Target Memory : LPDDR4

  1. Can we use the MC33PF8100CCES instead of the MC33PF8100FJES?
  2. Why does not recommend the OTP "CCES" version?
  3. If we use the CCES version, will it affect to the AP?

       I saw these device are different "power up time" with SW5 DDR power channel between MC33PF8100CCES and MC33PF8100FJES, and OTP version "CCES" is not recommended for new design  at PF8100 data sheet.

deega_jung_0-1654242391960.png

 

deega_jung_1-1654242392268.png

 

Thanks,

Deega

标签 (1)
0 项奖励
回复
1 解答
3,275 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi YOUNG KEE JUNG,

1. Can we use the MC33PF8100CCES instead of the MC33PF8100FJES?

[A] Yes, you can use the MC33PF8100CCES instead of the MC33PF8100FJES. The only technical difference is the timing as you have found in the OTP reports. The output voltages are the same. The target market for both is the Automotive.

2. Why does not recommend the OTP "CCES" version?

[A] NXP decided to discontinue this type, there is a business reason behind it. Not a technical reason. NXP does not recommend the part be designed into new end products. No discontinuance decision has been made, and all minimum longevity commitments will be honored. When a decision is made, it will be communicated through NXP's product discontinuance process.

3. If we use the CCES version, will it affect to the AP?

[A] Only the SW5 will turn on later. If this is not crucial for your application, then it will not affect it.

With Best Regards,

Jozef

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,276 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi YOUNG KEE JUNG,

1. Can we use the MC33PF8100CCES instead of the MC33PF8100FJES?

[A] Yes, you can use the MC33PF8100CCES instead of the MC33PF8100FJES. The only technical difference is the timing as you have found in the OTP reports. The output voltages are the same. The target market for both is the Automotive.

2. Why does not recommend the OTP "CCES" version?

[A] NXP decided to discontinue this type, there is a business reason behind it. Not a technical reason. NXP does not recommend the part be designed into new end products. No discontinuance decision has been made, and all minimum longevity commitments will be honored. When a decision is made, it will be communicated through NXP's product discontinuance process.

3. If we use the CCES version, will it affect to the AP?

[A] Only the SW5 will turn on later. If this is not crucial for your application, then it will not affect it.

With Best Regards,

Jozef

0 项奖励
回复
3,271 次查看
deega_jung
Contributor III

Hi Jozef,

Thank you for your comment.

I'll close this issue.

Thanks,

Deega

0 项奖励
回复