PF8100CCES Feasibility

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PF8100CCES Feasibility

Jump to solution
3,267 Views
deega_jung
Contributor III

Hi,

Target AP : MIMX8QX1AVLFZAC

Target Memory : LPDDR4

  1. Can we use the MC33PF8100CCES instead of the MC33PF8100FJES?
  2. Why does not recommend the OTP "CCES" version?
  3. If we use the CCES version, will it affect to the AP?

       I saw these device are different "power up time" with SW5 DDR power channel between MC33PF8100CCES and MC33PF8100FJES, and OTP version "CCES" is not recommended for new design  at PF8100 data sheet.

deega_jung_0-1654242391960.png

 

deega_jung_1-1654242392268.png

 

Thanks,

Deega

Labels (1)
0 Kudos
Reply
1 Solution
3,263 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi YOUNG KEE JUNG,

1. Can we use the MC33PF8100CCES instead of the MC33PF8100FJES?

[A] Yes, you can use the MC33PF8100CCES instead of the MC33PF8100FJES. The only technical difference is the timing as you have found in the OTP reports. The output voltages are the same. The target market for both is the Automotive.

2. Why does not recommend the OTP "CCES" version?

[A] NXP decided to discontinue this type, there is a business reason behind it. Not a technical reason. NXP does not recommend the part be designed into new end products. No discontinuance decision has been made, and all minimum longevity commitments will be honored. When a decision is made, it will be communicated through NXP's product discontinuance process.

3. If we use the CCES version, will it affect to the AP?

[A] Only the SW5 will turn on later. If this is not crucial for your application, then it will not affect it.

With Best Regards,

Jozef

View solution in original post

0 Kudos
Reply
2 Replies
3,264 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi YOUNG KEE JUNG,

1. Can we use the MC33PF8100CCES instead of the MC33PF8100FJES?

[A] Yes, you can use the MC33PF8100CCES instead of the MC33PF8100FJES. The only technical difference is the timing as you have found in the OTP reports. The output voltages are the same. The target market for both is the Automotive.

2. Why does not recommend the OTP "CCES" version?

[A] NXP decided to discontinue this type, there is a business reason behind it. Not a technical reason. NXP does not recommend the part be designed into new end products. No discontinuance decision has been made, and all minimum longevity commitments will be honored. When a decision is made, it will be communicated through NXP's product discontinuance process.

3. If we use the CCES version, will it affect to the AP?

[A] Only the SW5 will turn on later. If this is not crucial for your application, then it will not affect it.

With Best Regards,

Jozef

0 Kudos
Reply
3,259 Views
deega_jung
Contributor III

Hi Jozef,

Thank you for your comment.

I'll close this issue.

Thanks,

Deega

0 Kudos
Reply