PF3000 alternative packages

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PF3000 alternative packages

跳至解决方案
3,637 次查看
jeroenvanderlaa
Contributor III

Hi there,

we have a board with an i.MX6SX. We use the MC32PF3000A5EP as a PMIC for this board. This specific PMIC has availability problems at the moment. When I look in the datasheet of the PF3000 I see that the MC33PF3000A5ES and the MC34PF3000A5ES are also viable options. The only difference I can find is that the latter 2 are automotive and industrial grade resp.

When I use the product selector for PMIC's (https://www.nxp.com/products/product-selector:PRODUCT-SELECTOR#/category/c757_c1820_c219) these latter 2 are not available when I select the i.MX6SX as a processor. Is this just an error in the selector or can I safely use these components interchangeably?

 

Best regards,

Jeroen van der Laan

标签 (2)
标记 (1)
0 项奖励
回复
1 解答
3,620 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Jeroen van der Laan,

Yes, you can use the MC33PF3000A5ES and the MC34PF3000A5EP interchangeable replacements for the MC32PF3000A5EP. I would recommend the MC34PF3000A5EP (Industrial), because it shares the same package as the MC32PF3000A5EP (consumer), while the MC33PF3000A5ES (automotive) have a little different package (wettable flank).

Maybe the reason why you cannot find them in the product selector when i.MX6SX is selected, is because A5 programmed version is for the i.MX6SL as you can see in table 1 of the PF3000 datasheet: https://www.nxp.com/docs/en/data-sheet/PF3000.pdf

Programmed versions A3 and A4 are made for i.MX6SX.

Regards,

Jose

 

在原帖中查看解决方案

2 回复数
3,621 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Jeroen van der Laan,

Yes, you can use the MC33PF3000A5ES and the MC34PF3000A5EP interchangeable replacements for the MC32PF3000A5EP. I would recommend the MC34PF3000A5EP (Industrial), because it shares the same package as the MC32PF3000A5EP (consumer), while the MC33PF3000A5ES (automotive) have a little different package (wettable flank).

Maybe the reason why you cannot find them in the product selector when i.MX6SX is selected, is because A5 programmed version is for the i.MX6SL as you can see in table 1 of the PF3000 datasheet: https://www.nxp.com/docs/en/data-sheet/PF3000.pdf

Programmed versions A3 and A4 are made for i.MX6SX.

Regards,

Jose

 

3,613 次查看
jeroenvanderlaa
Contributor III

Thanks Jose,

the confusion for me is that that the MC32PF3000A5EP does show up as an i.MX6SX compatible PMIC in the product selector where the MC33 and MC34 counterparts do not. I notice that the product selector indicates that the MC33/MC34 parts do not have a boost regulator, this does not show in the data sheet (as far as I can see). I presume the boost regulator is there, can you confirm that?

Is it possible to change this in the product selector to prevent confusion for future users?

Best regards,

Jeroen van der Laan

 

0 项奖励
回复