PF3000 Programming

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PF3000 Programming

跳至解决方案
5,053 次查看
niteshsahay
Contributor III

Hi

While programming PF3000 i am getting error and PMIC ic not getting programmed.

In GUI in configuration section i have highlighted the desired values for my application and saved then i loaded the configuration and programmed the PMIC which in result shows error saying PMIC not programmed.

Is there anything i need to do in scrip editor.

I have attached the error for the reference.

pastedImage_3.png

Regards

Nitesh

1 解答
4,857 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Nitesh,

 

From the image you sent, it seems like no device is detected, this should be the main reason of the problem, please check that you are properly placing the PMIC inside the socket.

Another possible cause could be that the devoice you are using is an already programmed device (you need to use a PF3000A0 unprogrammed version to be able to OTP program your PMIC) according to the “ECC Error” that appear in your log window.

 

There is a detailed video that shows how to OTP program the PF3000 PMIC using the GUI, you can find this video in the following link: http://www.nxp.com/video/:PF3000-PROGRAMMING-OTP


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
4,743 次查看
shashank1
Contributor III

Hi,

How do I verify the programed voltages? 

Using the programmer board and EVB board like the shown in attached image? 

0 项奖励
回复
4,858 次查看
reyes
NXP TechSupport
NXP TechSupport

Hi Nitesh,

 

From the image you sent, it seems like no device is detected, this should be the main reason of the problem, please check that you are properly placing the PMIC inside the socket.

Another possible cause could be that the devoice you are using is an already programmed device (you need to use a PF3000A0 unprogrammed version to be able to OTP program your PMIC) according to the “ECC Error” that appear in your log window.

 

There is a detailed video that shows how to OTP program the PF3000 PMIC using the GUI, you can find this video in the following link: http://www.nxp.com/video/:PF3000-PROGRAMMING-OTP


Have a great day,
Jose

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------