PF1510 EVK GUI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PF1510 EVK GUI

3,497件の閲覧回数
russl
Contributor II

The PF1510_GUI_x64_Installer fails with error message that no JRE could be found. The requirements do not mention anything about needing a JRE. What version is needed? Will an Open JDK installation work? If so, what setup (reg keys etc. so installer can find the open JDK installation) is required for it to work? Or does this installer and resulting program need some JAVA browser plugin?

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

3,490件の閲覧回数
russl
Contributor II

Thank you for the response guoweisun. I was hoping there was a way to use the JRE in OpenJDK. Can you comment on this matter at all?

0 件の賞賛
返信

3,489件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

For you side only install the Java JRE the GUI program will automatically call it when open this GUI.

0 件の賞賛
返信

3,487件の閲覧回数
russl
Contributor II

I understand I only need the JRE. But, as I have said twice now, I want to use the Open version, not the one referenced in the link you sent. Is this possible?

0 件の賞賛
返信

3,482件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

You can try to the open version but I usual download from the link and it works.

0 件の賞賛
返信

3,492件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

You can refer to below for Installing the Java JRE:

  1. Download Java JRE (Java SE Runtime Environment), available at http://

www.oracle.com/technetwork/java/javase/downloads/jre8-downloads-2133155.html

(8u162 or newer).

  1. Open the installer and follow the installation instructions.
  2. Following the successful installation, restart the computer.
0 件の賞賛
返信